Technical FAQs

Ask a Question

How far into the wall does a SU2040M150R install?

This device is a Reverse All-In-One, providing a meter socket and main lugs section on the exterior of the building and a main breaker load center on the interior of the building. It is 7.9`` deep. Of the 7.9``, 3.5`` will extend past the semi-flush flange (outside surface of the stud wall), 3.5`` will be in the wall cavity and .9`` will extend past the interior surface of the stud wall. Please refer to Approval Drawing #1965 for dimensional details.

CTA-ID : 2036068
Was this helpful?
What can we do to improve the information ?