Technical FAQs

Ask a Question

Why is there a make and break current rating?

The rated making capacity is important because if exceeded can lead to major failure such as welding of contacts.
If the breaking current is exceeded it is difficult or impossible to extinguish the arc and cause excessive wear or failure.


CTA-ID : 2036049
Was this helpful?
What can we do to improve the information ?