Technical FAQs

Ask a Question

What is the difference between the GK1** and the GK1**U with the U suffix?

The GK1DDU has the UL marking on the device.


CTA-ID : 2035943
Was this helpful?
What can we do to improve the information ?