Technical FAQs

Ask a Question

Is an EZM11000CB main device available with a 900 A main circuit breaker factory installed?

Yes ....Order this Special device on Lexington as an EZM11000CB900. List price is the same as the standard 1000A device, allow 4 to 6 weeks for shipment from Rojo Gomez, Mexico. A special MHF36900 main circuit breaker will be factory installed in this device prior to shipping.


CTA-ID : 2036017
Was this helpful?
What can we do to improve the information ?