Technical FAQs

Ask a Question

What are the repair parts for the CHU361AWK, series F5? (may be shown as F05)

The replacement parts for the CHU361AWK, series F5 (F05) are as follows. No other parts are available.

Line Base Assembly - 40566-430-50 (requires one per switch. Arc suppressor assembly not included)
Arc Suppressor Assembly - 40566-694-51 (requires one per switch)
Lug Assembly - CL0306F (includes 6 lugs)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Handle Gasket - 40566-031-01
Lockplate - 40566-376-01
Line base mounting screw - 40205-160-01 (3 required)
Arc Suppressor mounting screw - 40205-145-01 (1 required)
Lockplate mounting screw - 22999-405-62 (2 required)


CTA-ID : 2035719
Was this helpful?
What can we do to improve the information ?