Technical FAQs

Ask a Question

What is the terminal lug data for the 82255 and 82255R Double Throw Safety Switches?

The lugs on these devices will accept (1) #1/0 - 600 kcmil AL or CU conductors per phase or (2) #1/0 - 300 kcmil AL or CU conductors per phase.


CTA-ID : 2035114
Was this helpful?
What can we do to improve the information ?