Technical FAQs

Ask a Question

What is the part number for the grease, anti-oxidant or lubricant that can be used for the terminals on our dry type transformers?

Any electrical approved joint compound rated for AL/CU use with a thermal rating greater than 90 degrees C is suitable. Square D applies such a coumpound to the terminals of its aluminum wound transformers but does not offer it as a post-purchase item


CTA-ID : 2035186
Was this helpful?
What can we do to improve the information ?