Technical FAQs

Ask a Question

Is there a filler plate available to close off the openings for the tenant breaker handles in the covers of a MPR85200?

No filler plate is available to close off the tenant breaker handle openings in this MPR85200 device. Padlock provisions are provided to lock the hinged plastic doors supplied on the front covers of this unit for each tenant breaker position (padlock to be supplied separately).


CTA-ID : 2035944
Was this helpful?
What can we do to improve the information ?