Technical FAQs

Ask a Question

What do the different numbers K2, K3, K4 etc. indicate on the 9003 K cam switches?

The different K numbers indicate the different size contacts with different current and voltage ratings. However, we no longer offer custom order 9003 cam switches other than the 9003K2. In place of 9003K3 to 9003K9 we offer K32 (32A) thru K150 (150A) cam switches, but it is a limited offer of built up switches. See 9003CT0402.


CTA-ID : 2035830
Was this helpful?
What can we do to improve the information ?