Technical FAQs

Ask a Question

Can a 8501RSD4* be used to switch an AC load ?

Yes , up to 240vac 10 amp max resistive or general use or 120vac 15amp max resistive .


CTA-ID : 2035966
Was this helpful?
What can we do to improve the information ?