Technical FAQs

Ask a Question

In selecing a NQOD442L225CU merchandise panel interior, is the solid neutral copper also along with the bus?

No the neutral is aluminum. To get copper neutral panel has to factory assembled.


CTA-ID : 2035949
Was this helpful?
What can we do to improve the information ?