Technical FAQs

Ask a Question

What are the part numbers for the replacement lugs on a PTB502G tap box?

Issue:
What are the part numbers for the replacement lugs on a PTB502G tap box?

Product Line:
Busway.

Environment:
Products sold in the United States.

Cause:
Maintenance.

Resolution:
The lug part numbers and quantity required for this unit are shown below:
2) 40251-162-51 B & N Phase Lug
2) 40251-160-51 A & C Phase Lug
1) 40251-042-50 Ground Lug



CTA-ID : 2035919
Was this helpful?
What can we do to improve the information ?