Technical FAQs

Ask a Question

What is used with the ZB4 and ZB5 potentiometers as legend plates?

Issue:
What is used with the ZB4 and ZB5 potentiometers as legend plates?

Product Line:
Harmony Pushbuttons

Environment:
All Products

Cause:
Product Features

Resolution:
There are graduations and a pointer on the knob, and the standard legends are compatible with these potentiometer operators.


CTA-ID : 2035977
Was this helpful?
What can we do to improve the information ?