Technical FAQs

Ask a Question

What is the catalog number for a 9001Type K Pilot Light for 277 volts?

Issue:
What is the catalog number for a 9001Type K Pilot Light for 277 volts?

Product Line:
Harmony Push Buttons

Environment:
Harmony 30mm

Cause:
Product Selection

Resolution:
The catalog number is 9001KP8 which has a 277 volt AC transformer pilot light, however the colored lens is not supplied with this.
You can get a plastic fresnel lens (A31 is amber, blue - L31, clear - C31, green - G31, red - R31, white - W31 or Yellow Y31),
Plastic domed lens (A9 is amber, blue- L9, clear - C9, green - G9, red - R9, white - W9 or yellow - Y9),
or glass lens (A6 is amber, blue - L6, clear - C6, green - G6, red - R6, white - W6 or yellow - Y6) by inserting the correct suffix.


CTA-ID : 2035975
Was this helpful?
What can we do to improve the information ?