Technical FAQs

Ask a Question

Is a 8`` to 4`` reducer available for LDB type wireway?

No. A 8`` to 4`` reducer is not available, however, this can be acomplished by combining a LDB86R (8`` to 6`` reducer), a LDB61 (1 foot length of 6`` wireway) and a LDB64R (6`` to 4`` reducer).


CTA-ID : 2035776
Was this helpful?
What can we do to improve the information ?