Technical FAQs

Ask a Question

Bus screw for QOB breaker

Issue:  
What is the B screw for a QOB type breaker?

Product Line:
QOB

Resolution:
The part number for the screw is 48820-020-01, and it is available in Q2C.
Screw size is 10-32


CTA-ID : 2035760
Was this helpful?
What can we do to improve the information ?