Technical FAQs

Ask a Question

Is there another part number that is available in stock that is similar to catalog number 8010302653? It is a copper ground bar.

The PK27GTA aluminum ground bar is similar to the copper ground bar 8010302653. The PK27GTA is readily available.


CTA-ID : 2035746
Was this helpful?
What can we do to improve the information ?