Technical FAQs

Ask a Question

Can the QO or HOM Homeline arc fault breaker AFI be used with a 2 wire circuit?

Yes. As long as there is not a shared neutral and the neutral is grounded at the service entrance only.

CTA-ID : 2035914
Was this helpful?
What can we do to improve the information ?