Technical FAQs

Ask a Question

Is a 240V version of the H or J PowerPact breaker available? Is part number JDA32250 a valid catalog number?

No. The H and J frame breakers are not made in a 240 volt version. Use a JDA36250 600V rated circuit breaker in this application.

CTA-ID : 2035909
Was this helpful?
What can we do to improve the information ?