Technical FAQs

Ask a Question

Is the generator interlock kit, K-5010, K-5011, K-5210, K-5310, K-5410, K-9010, K-9110 or K-9310 for QO and Homeline loadcenters, a Square D product?

Issue:
Selection

Product Line:
Load Center Accessory

Cause:
Clarification of selection of generator interlock kit

Resolution:
These generator interlock kits are manufactured by Generator Interlock Technologies in Richmond, VA. Generator Interlock Technologies is NOT affiliated with Schneider Electric nor Square D Company. They offer various load center interlock kits for all the major load center manufacturers. This is not a Square D product. The use of a third party generator interlock kit would not be listed in our UL files, nor listed for use on the load center accessories list noted on the load center wiring diagram, nor covered by the Square D Warranty.


CTA-ID : 2035874
Was this helpful?
What can we do to improve the information ?