Technical FAQs

Ask a Question

How many anchor bolts have to be used in a lineup of switchgear?

If the lineup has seismic requirements, then all anchor bolts should be installed. (4 per vertical section. Otherwise only the anchor bolts at the outside edges on either end of the lineup are required.


CTA-ID : 2035879
Was this helpful?
What can we do to improve the information ?