Technical FAQs

Ask a Question

Does the push to trip function of a NW30 3000A breaker work at a breaker loading lower than 20-25%?

The push to trip function, similar to the LCD display, also requires either 20-25% loading of the breaker, or 24V auxiliary power at the auxiliary terminals to become functional.

CTA-ID : 2035710
Was this helpful?
What can we do to improve the information ?