Technical FAQs

Ask a Question

What is the temperature rating for the 9007C54K limit switch?

The standard limit switch is rated for -20 degree F to 184 degree F If the customer can use 9007FA3 or 9007FA4 spring rods, Form Y128 allows operation to -40 degrees F.


CTA-ID : 2035854
Was this helpful?
What can we do to improve the information ?