Technical FAQs

Ask a Question

Is the KA26125 I-Line circuit breaker rated for DC?

Issue:
Is the KA26125 I-Line circuit breaker rated for DC?

Product Line:
Panelboards.

Environment:
Products made in the United States.

Cause:
Product features.

Resolution:
It is rated 10KA at 250VDC


CTA-ID : 2035915

Was this helpful?
What can we do to improve the information ?