Technical FAQs

Ask a Question

Is there a provision to order an EZM1800CB, 800 ampere main breaker unit with a 700A breaker factory installed?

Yes, we have made arrangements with the Mechanicsburg Mod Center to offer a special EZM 700A main by starting with a standard EZM3800CB and a standard MHL36700 main breaker. We remove the 800A breaker from the EZM main and replace it with the 700A breaker prior to shipping. This normally takes 1 to 2 week to accomplish, and both items must be in stock to start the modification.


CTA-ID : 2035844
Was this helpful?
What can we do to improve the information ?