Technical FAQs

Ask a Question

What are the restrictions to mounting QOB3110VH and larger branch breakers in a NQOD panelboard?

The QOB3110VH through QOB3150VH requires 6 vertical spaces and the largest branch breaker which can be mounted adjacent to (across from) it is 20A.

CTA-ID : 2035593
Was this helpful?
What can we do to improve the information ?