Technical FAQs

Ask a Question

What are the repair parts for the CHU361DS, series F5? (may be shown as F05)

The repair parts for the CHU361DS, series F5 (F05) are as follows. No other parts are available.
-Line Base Assembly - 40566-430-50 (arc suppressor not included)
-Line Base mounting screw - 40205-160-01 (3 required)
-Arc Suppressor Assembly - 40566-694-51
-Arc Suppressor mounting screw - 40205-145-01 (1 required)
-Lug Assembly - CL0306F (includes 6 lugs)
-Mechanism Assembly - 40566-107-50 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 40566-998-50
-Cover Interlock Defeat Coupling - 40566-997-50
-Handle Assembly - 40566-994-50 (also recommend replacing Lockplate Gaskets)
-Lockplate - 40566-932-01 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 40503-228-02 (2 required)
-Lockplate mounting screw - 21949-181-21 (2 required)
-Ground Lug - 40251-016-52 - (2 total required)
-Ground Lug Mounting Screw - 40205-135-03



CTA-ID : 2035810
Was this helpful?
What can we do to improve the information ?