Technical FAQs

Ask a Question

Is there a longer Allen set screw available for the AL800MA7 lugs?

A longer Allen wire binding screw is not available, but the the pitch is 9/16-18 coarse thread and the screw is tin-plated aluminum.

CTA-ID : 2035791
Was this helpful?
What can we do to improve the information ?