Technical FAQs

Ask a Question

What is included in a 40562-118-50?

This kit is required to field install incoming line and neutral lugs on the 400A CSED devices. The kit consists of (6) 1/2`` keps nuts and (6) flat washers. Two keps nuts and washers are required to mount each phase (2) and neutral (1) lug. The lugs are purchased separately and field installed. This lug mounting kit is factory provided in the CSED device.


CTA-ID : 2035753
Was this helpful?
What can we do to improve the information ?