Technical FAQs

Ask a Question

What does the N12 in a Control Transformer catalog number designate? For example 9070TF50D20N12

The N12 option defines a ``Fusing 3 pole non-rejection (30 A max fuse)``. It is considered an OEM product with sales restricted to the OEMs. Contact the equipment manufacturer for replacment.

CTA-ID : 2035752
Was this helpful?
What can we do to improve the information ?