Technical FAQs

Ask a Question

Does Square D make a single phase 2 speed starter?

We do not manufacture as standard a 2 speed electromechanical starter ( Class 8810 ) for a single phase application. We do manufacture the 2512 type F manual starter or 2512K manual switch.

CTA-ID : 2035706
Was this helpful?
What can we do to improve the information ?