Technical FAQs

Ask a Question

Is it possible to change the battery of the MICROLOGIC control unit breaker?

Yes. The equipment and all control power to the breaker must be de-energized prior to taking the cover off. The battery (S33593) is then accessible on the left rear side of the control unit.

CTA-ID : 2035764
Was this helpful?
What can we do to improve the information ?