Technical FAQs

Ask a Question

9012GAW5: What is the maximum media temperature rating?

It is +120 Degree C, or +250 Degree F.  Use of a steam capillary of at least 10 ft in length, when properly applied, will allow monitoring of steam pressures up to 250psi, at  temperatures up to  400 degrees F.

CTA-ID : 2035736
Was this helpful?
What can we do to improve the information ?