Technical FAQs

Ask a Question

Does an LA400R circuit breaker enclosure provide the capability to padlock the circuit breaker handle in either the ON or OFF position?

The LA400R does not incorporate an externally operable handle, therefore the enclosure does not have the capability of locking the circuit breaker handle. The locking function can be accomplished by field installing a separately purchased HPALM handle padlock attachment to the installed LAL, LHL or Q4L breaker, or a HPAFK handle padlock attachment to the installed KAL or KHL breaker. Also, the front cover of the LA400R can be padlocked closed, preventing access to the enclosed breaker.


CTA-ID : 2034443
Was this helpful?
What can we do to improve the information ?