Technical FAQs

Ask a Question

On the 400A CSED Meter-Mains and All-In-One panels, what is the difference between the Series M02 and M03 designs?

Issue:
Product Features

Product Line:
CSED

Cause:
Clarification

Resolution:
The difference is the meter socket used. The Series M02 design used a meter socket that was purchased from Cooper B-Line (part number 21324CD). The Series M03 design is using a meter socket that is manufactured by Square D Company (part number 73294-902-50). The meter sockets are not compatible between the two different designs.


CTA-ID : 2034477
Was this helpful?
What can we do to improve the information ?