Technical FAQs

Ask a Question

Can the catalog number EZML332400 be shipped with only (1) factory installed tenant circuit breaker and only one meter socket position?

Current design

Product Line:
EZM Metering

Series M03 tenant breakers and meter sockets

Device Configuration.

For EZM branch device applications needing just one (1) 400A Type tenant circuit breaker and one Class 320 Lever Bypass type meter socket position, order catalog number EZML331400. The EZML331400 is a Single gang EZML type branch device designed to accommodate one 400A tenant breaker. We are not able to provide a 2-Gang 400A branch unit having only one Class 320, Lever Bypass type meter socket and one 400A Type tenant circuit breaker.

CTA-ID : 2032972
Was this helpful?
What can we do to improve the information ?