Technical FAQs

Ask a Question

What is the operating temperature range for the 9050AO timers?

The operating temperature range is from 10 degrees C to 60 degrees C (14 degrees F to 140 degrees F).


CTA-ID : 2034412
Was this helpful?
What can we do to improve the information ?