Technical FAQs

Ask a Question

What is the difference between model number XX7V1A1NAM12 and an XX7V1A1NBM12

The XX7V1A1NAM12 is NPN with a normally open output. The output will energize when a target is detected. The XX7V1A1NBM12 has an NPN output that DE-energizes when a target is detected. (Normally Closed logic)



CTA-ID : 2034408
Was this helpful?
What can we do to improve the information ?