Technical FAQs

Ask a Question

What is the life expectancy or endurance for the Powerpact M breaker?

UL testing is 500 operations under full load and 3000 operations under no load.


CTA-ID : 2034135
Was this helpful?
What can we do to improve the information ?