Technical FAQs

Ask a Question

What is the actual rating of a QOB200? Is it a breaker or a molded case switch? Is it a 200A device?

The QOB200 is a 2-pole non-automatic molded case switch, and is limited to 60A max in operation. It has no circuit protection capabilities, and is for switching circuits on or off only.


CTA-ID : 2034134
Was this helpful?
What can we do to improve the information ?