Technical FAQs

Ask a Question

Are Homeline load centers available with no knockouts?

Issue:
Product features

Product Line:
Homeline Load Center

Environment:
Type 1 Load Center

Cause:
Special feature request

Resolution:
Homeline load centers are not available without knockouts. If a panel without knockouts is required, consider using a NQ panelboard.


CTA-ID : 2034294
Was this helpful?
What can we do to improve the information ?