Technical FAQs

Ask a Question

Do the separately mounted Circuit Breaker Enclosures, such as the KA225F, KA225S, or KA225RB have a CE mark for use in European applications?

No. The separately mounted Circuit Breaker Enclosures have UL and CSA listing for use in North America, but no CE mark.


CTA-ID : 2034279
Was this helpful?
What can we do to improve the information ?