Technical FAQs

Ask a Question

What is the Neutral Assembly for a DU325 and/or DU325R safety switch?

Issue:
Selection

Product Line:
GD Safety Switch

Cause:
Selection of correct neutral assembly

Resolution:
A neutral assembly is not available for the DU325 or DU325R safety switch. If a neutral is required, consider using a Heavy Duty equivalent: HU365 or HU365R and H600SN neutral assembly. 


CTA-ID : 2034168
Was this helpful?
What can we do to improve the information ?