Technical FAQs

Ask a Question

Is the Vario switch defeatable?

The real question should be - Is the handle defeatable? The answer is NO. This is a UL508 switch. Only UL98 switches are required to have defeatable handles.

CTA-ID : 2034109
Was this helpful?
What can we do to improve the information ?