Technical FAQs

Ask a Question

What is the Filler Plate to fill the KDL main circuit breaker opening in a QO342M150 cover (QOC342MF or QOC342MS)?

Issue:
Selection

Product Line:
QO Load Center

Environment:
Selection

Cause:
Select correct filler plate

Resolution:
The Filler Plate is catalog number KFP. (2/5/15 update - KFP is now obsolete and no longer available).


CTA-ID : 2034339
Was this helpful?
What can we do to improve the information ?