Technical FAQs

Ask a Question

Why is there a .5`` gap between the end of the connector and the main bus when trying to connect the N150MH main breaker adapter kit.

Always put the adapter kit on the same end as the solid neutral. Don`t tighten the connector links until every thing is assembled.

CTA-ID : 2034100
Was this helpful?
What can we do to improve the information ?