Technical FAQs

Ask a Question

What are the Nema 7 & 9 Class and Division ratings for the 2510MBR and 2510MCR type starters?

Enclosure Type: NEMA 7 & 9 Cast Iron
Hazardous Locations:
Class I Division 1 and 2, Groups C, D
Class II Division 1 and 2, Groups E, F, G


CTA-ID : 2034145
Was this helpful?
What can we do to improve the information ?