Technical FAQs

Ask a Question

What is the bus material used in the branch breaker distribution section of a SC1624M100S?

Issue:
Product Design Features

Product Line:
Combination Service Entrance Devices

Environment:
Bus rating

Cause:
Application

Resolution:
The bus material is tin plated aluminum. The SC1624M100S uses a Homeline load center interior and all Homeline interiors contain tin plated aluminum bussing.

 
Was this helpful?
What can we do to improve the information ?