Technical FAQs

Ask a Question

What are the torque specs for the Main Lug Wire binding Screws on a CH323AWK?

Issue:
Main lug torque specifications

Product Line:
Heavy Duty Safety Switches

Cause:
Installation

Resolution:

The torque specs are as follows:
#10 - 14 = 35 in-lbs
#8 = 40 in-lbs
#4-6 = 45 in-lbs
#1/0 - 3 = 50 in-lbs


CTA-ID : 2034189
Was this helpful?
What can we do to improve the information ?