Technical FAQs

Ask a Question

What is the torque value for the AL2500RK lug?

The wire binding screw is 46 foot pounds and the lug mounting nut 50 foot pounds. See instruction bulletin 48049-255-02, in the Technical library.

CTA-ID : 2034200
Was this helpful?
What can we do to improve the information ?